ADMS Patch Integration

The ADMS Patch Integration tab provides information about the Patch Packet generated by ArcFM and sent to the ADMS. This information is helpful for monitoring and, if necessary, trouble-shooting the process.

IMPORTANT:
  • The information on the ADMS Patch Integration tab is read-only.

  • This tab is present only for customers with the ADMS Patch Integration functionality.


The fields displayed include:

  • ID: A GUID that can be used to retrieve the resource from the Storage Service.

  • Design ID: A unique identifier for the Design Resource associated with the Patch.

  • Affected Subnetworks: A collection of all subnetwork names affected by the Patch.

  • Initial GRR Group Storage ID: The storage ID for the GeodatabaseRegionGroupResource that contains the initial state of GRRs for all subnetworks in the Patch.

  • Final State GRR Group Storage ID: The storage ID for the GeodatabaseRegionGroupResource that contains the final design state of GRRs for all subnetworks in the Patch.

  • Last Modified: The timestamp for the last update to the Patch Packet metadata resource.

  • Patch Status: A status for the Patch, based on information available to the ArcFM system from internal workflows and messages from ADMS. The application includes the following statuses out of the box, but more can added by your implementation team:

    • Approved

    • Closed

    • Confirmed

    • Created

    • Error

    • In Design

    • Rejected

    • Sent to ADMS

    • Sent to GIS For Sync

    • Unknown

  • Error Message: A short description of the error associated with the Patch Packet. If the Patch has no errors, this row does not appear in the display.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.