NonSpatialFeederSourceResource

Resource used to represent a feeder source network component that does not have a spatial representation.

Name

Type

Description

componentType

String

"NonSpatialFeederSource"

workflowState

Int32

[Existing, AsBuilt, Proposed, Undefined, Modified]

properties

IDictionary

Additional properties

id

Guid

Unique identifier

operatingVoltage

Voltage

Operating voltage

voltageClass

Int32

[Primary, Secondary, Unknown]

feederId

String

Feeder identifier

distributionSystemType

Int32

[Overhead, Underground, Submersible]

facilityId

String

Facility identifier

energizedPhases

Int32

[None, C, B, BC, A, AC, AB, ABC, Unknown]

closedPhases

Int32

[None, C, B, BC, A, AC, AB, ABC, Unknown]

sourceFeatureId

Guid

Source feature identifier

energySource

EnergySourceResource

Energy source

lifecycleStatusType

LifecycleStatusType

Lifecycle status

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.