UndergroundPolygonStructureResource

General purpose underground structure polygon component intended to be mapped to all underground structure polygon features.

Name

Type

Description

componentType

String

"UndergroundPolygonStructure"

workflowState

Int32

[Existing, AsBuilt, Proposed, Undefined, Modified]

properties

IDictionary

Additional properties

id

Guid

Unique identifier

geometry

IBoundedObject

Geometric representation

facilityId

String

Facility identifier

esriId

Int64

Esri identifier

type

String

Type of structure

isSubstation

Boolean

Indicates if it's a substation

subnetworkName

String

Subnetwork name

lifecycleStatusType

LifecycleStatusType

Lifecycle status

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.