GIS Schema

The schema is a crucial piece of the application’s architecture. It is the key “translator” that allows the application to understand the unique architecture and attributes of your company’s data. The attribute fields that end up in the Geodatabase Regions (GRRs) are determined via the GIS Schema mapping.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.