ElectricNetworkComponentWithTerminalsResource

Generic component class that represents a variety of non-switchable phased electric components that are either uncommon enough that we don't have detailed specification data, or simple enough that they don’t need detailed specification data.

When units in the UN are drawn spatially, they are contained by Assemblies, and the Components to use are:

  • ElectricNetworkComponentWithTerminalsResource — this is the unit.

  • ElectricNetworkComponentAssemblyResource — this is the assembly.

This differs from units in the UN that are non-spatially drawn. In those cases, the units are contained by Banks, and the Components to use are:

  • ElectricNetworkComponentUnitResource — this is the unit

  • ElectricNetworkComponentBankWithTerminalsResource — this is the bank.

IMPORTANT: One exception is Conductors, for which the modeling didn’t change between the UN and GN. ConductorBank and Conductor should be used in both because they don’t have terminals in the UN, plus the pattern of assemblies and of drawn units as devices doesn’t apply.

Name

Type

Description

componentType

String

"ElectricNetworkComponentWithTerminals"

workflowState

Int32

[Existing, AsBuilt, Proposed, Undefined, Modified]

properties

IDictionary

Additional properties

id

Guid

Unique identifier

operatingVoltage

Voltage

Operating voltage

voltageClass

Int32

[Primary, Secondary, Unknown]

distributionSystemType

Int32

[Overhead, Underground, Submersible]

geometry

IBoundedObject

Geometric representation

terminals

IEnumerable

List of terminals

specId

Guid

Specification identifier

esriId

Int64

Esri identifier

energizedPhases

Int32

[None, C, B, BC, A, AC, AB, ABC, Unknown]

phases

Int32

[None, C, B, BC, A, AC, AB, ABC, Unknown]

facilityId

String

Facility identifier

assemblyId

Guid

Assembly identifier

subnetworkName

String

Subnetwork name

lifecycleStatusType

LifecycleStatusType

Lifecycle status

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.