Create a Geodatabase Region

Follow these steps to create a GRR:

  1. On the Mapping tab, select Geodatabase Regions from the menu.

  2. Click the Add button.

  3. Search for and select subnetworks. You can click an individual subnetwork to highlight it or use the Shift and Ctrl keys to select multiple subnetworks.

    A list of subnetworks, across all tiers of the Utility Network that do not yet have a GRR created, is provided. You can search by typing in part of the name of the subnetwork. Then, press Enter or click Search. It is a keyword-style search that queries anywhere within the name.

    NOTE: Dirty subnetworks are filtered out from this view.

  4. Once they are highlighted, click Save. A notification is provided when the process is complete.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.