PoleResource

Component type used to represent Pole support structures.

Name 

Type 

Description 

componentType 

String 

"Pole" 

id 

Guid 

Unique identifier

esriId 

Int64 

Esri identifier

facilityId 

String 

Facility identifier

specId 

Guid 

Specification identifier

geometry 

IBoundedObject 

Geometric representation

workflowState 

Int32 

[Existing, AsBuilt, Proposed, Undefined, Modified] 

properties 

IDictionary 

Additional properties

lifecycleStatusType 

LifecycleStatusType 

Lifecycle status

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.