DistributedGeneratorWithTerminalsResource – Distributed Generator

A generalized generation unit, typically located on feeders and of small power.

Typical examples include: inverter-connected solar farms, wind-powered units or small farms, as well as small hydro or gas units, for which detailed modeling is not required.

Name

Type

Description

efficiency

Int32

Efficiency rating

ratedCosPhi

Double

Rated power factor

ratedPower

ApparentPower

Rated apparent power

ratedVoltage

Voltage

Rated voltage

faultContribution

Int32

Fault contribution

fuelType

FuelType

Type of fuel

grounded

Boolean

Grounded status

islandOperation

Boolean

Island operation capability

regulators

List

List of regulators

componentType

String

"DistributedGeneratorWithTerminals"

workflowState

Int32

[Existing, AsBuilt, Proposed, Undefined, Modified]

properties

IDictionary

Additional properties

id

Guid

Unique identifier

operatingVoltage

Voltage

Operating voltage

voltageClass

Int32

[Primary, Secondary, Unknown]

distributionSystemType

Int32

[Overhead, Underground, Submersible]

geometry

IBoundedObject

Geometric representation

terminals

IEnumerable

List of terminals

assemblyId

Guid

Assembly identifier

esriId

Int64

Esri identifier

energizedPhases

Int32

[None, C, B, BC, A, AC, AB, ABC, Unknown]

phases

Int32

[None, C, B, BC, A, AC, AB, ABC, Unknown]

facilityId

String

Facility identifier

subnetworkName

String

Subnetwork name

lifecycleStatusType

LifecycleStatusType

Lifecycle status

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.