Default Values for Designer XI Fields

Designer XI and Feeder Services leverage the same Geodatabase Region (GRR) functionality. There are two fields provided in the GRR that only apply to Designer XI:

  • Distribution System Type

  • Voltage Class

Because Feeder Services does not currently use these fields, and thus does not have anything to populate them, the GRR automatically defaults to “Overhead” for Distribution System Type and “Primary” for Voltage Class.

In sum, for the purposes of Feeder Services, these fields and their values can be ignored in the GRR.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.