VoltageRegulatorAssemblyResource

Assembly containing VoltageRegulatorWithTerminalsResource devices.

Name

Type

Description

distributionSystemType

Int32

Overhead, Underground, Submersible

esriId

Int64

Esri identifier

deviceIds

IEnumerable\<Guid>

List of device identifiers

facilityId

String

Facility identifier

componentType

String

VoltageRegulatorAssembly

id

Guid

Unique identifier

workflowState

Int32

Existing, AsBuilt, Proposed, Undefined, Modified

properties

IDictionary

Additional properties

geometry

IBoundedObject

Geometric representation

subnetworkName

String

Subnetwork name

lifecycleStatusType

LifecycleStatusType

Lifecycle status

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?