Tables

In the Tables portion of the schema, you map the Feeder Services fields to their equivalent fields in the geodatabase. In short, when the application creates a Geodatabase Region (GRR), the Tables portion determines which fields for which features/objects are included in the GRR.

If applicable, you can map the fields for all Asset Groups of a feature class, or you can create multiple Table mappings in order to separate out certain Asset Groups.


Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.