ConductorBankResource

A container for one or more conductor banked components.

Name 

Type 

Description 

componentType 

String 

"ConductorBank" 

facilityId 

String 

Facility identifier

complexEdgeId 

Guid 

Unique ID of a complex edge conductor bank. The Complex Edge feature allows, for example, distribution transformers to tap power from any arbitrary location along the length of a Primary (i.e., MV) conductor feature without having to artificially split the conductor feature at each transformer location to become two conductor features.

deviceIds 

IEnumerable 

List of device identifiers

neutralConductorId 

Guid 

Unique ID of a neutral conductor. This is populated if a neutral conductor exists.

geometry 

IBoundedObject 

Geometric representation

workflowState 

Int32 

[Existing, AsBuilt, Proposed, Undefined, Modified] 

id 

Guid 

Unique identifier

esriId 

Int64 

Esri identifier

measuredLength 

Double 

Measured length of the conductor bank resource

measuredLengthWithUnit 

Length 

Measured length with the unit of the conductor bank resource

properties 

IDictionary 

Additional properties

operatingVoltage 

Voltage 

Operating voltage

voltageClass 

Int32 

[Primary, Secondary, Unknown] 

distributionSystemType 

Int32 

[Overhead, Underground, Submersible] 

energizedPhases 

Int32 

[None, A, B, C, AB, AC, BC, ABC, Unknown] 

subnetworkName 

String 

Subnetwork name

assemblyId 

Guid 

Assembly identifier

lifecycleStatusType 

LifecycleStatusType 

Lifecycle status

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.