Utility Network with Spatial Units

When units in the UN are drawn spatially, they are contained by Assemblies, and the Components used are:

  • ElectricNetworkComponentWithTerminalsResource — this is the unit.

  • ElectricNetworkComponentAssemblyResource — this is the assembly.

IMPORTANT: One exception is Conductors, for which the modeling didn’t change between the UN and GN. ConductorBank and Conductor should be used in both because they don’t have terminals in the UN, plus the pattern of assemblies and of drawn units as devices doesn’t apply. For more information about configuring Assembly feature classes, refer to the Composite Equipment Feature Details topic in the ArcFM UN Configuration Guide.

A UN model with spatial units suffers from performance issues that significantly impact network tracing, editing, versioning, etc.

Schneider Electric supports this particular model for existing customers, but we strongly discourage its use entirely.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.