NonSpatialServiceLocationWithTerminalsResource

Represents a service location as an electric junction that does not have a spatial representation.

This resource is typically used in an urban environment here: premises represents a tall building/skyscraper, which is mapped to the ServicePointWithTerminalsResource and it is connected to different layers/floors, layers/floors are considered as separate service locations that are mapped to NonSpatialServiceLocationWithTerminalsResource and are connected to multiple meters, meter represents a single consumption point and is mapped to NonSpatialMeterWithTerminalsResource.

Name

Type

Description

componentType

String

"NonSpatialServiceLocationWithTerminals"

workflowState

Int32

[Existing, AsBuilt, Proposed, Undefined, Modified]

properties

IDictionary

Additional properties

id

Guid

Unique identifier

operatingVoltage

Voltage

Operating voltage

voltageClass

Int32

[Primary, Secondary, Unknown]

distributionSystemType

Int32

[Overhead, Underground, Submersible]

terminals

IEnumerable

List of terminals

assemblyId

Guid

Assembly identifier

esriId

Int64

Esri identifier

energizedPhases

Int32

[None, C, B, BC, A, AC, AB, ABC, Unknown]

phases

Int32

[None, C, B, BC, A, AC, AB, ABC, Unknown]

facilityId

String

Facility identifier

subnetworkName

String

Subnetwork name

lifecycleStatusType

LifecycleStatusType

Lifecycle status

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.