Mapping

 After operational maps are configured in the Mapping plugin, they are then available for further configuration in each XI series application’s plugin.

On the Mapping tab in the Feeder Services plugin are two sections, Maps and Geodatabase Regions (GRRs).

  • Maps – Feeder Services uses a selected map to create and update GRRs, and inform the application of your low voltage (LV) subnetworks to group within the GRR.

  • Geodatabase Regions – Feeder Services allows you to group LV subnetworks together in the same GRR export, rather than export them in separate GRRs.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.