VoltageRegulatorWithTerminalsResource

This resource is a component of the distribution system that ensures a steady constant voltage supply through all operational conditions. It regulates voltage during power fluctuations and variations in loads.

Name

Type

Description

componentType

String

VoltageRegulatorWithTerminals

workflowState

Int32

Existing, AsBuilt, Proposed, Undefined, Modified

properties

IDictionary

Additional properties

id

Guid

Unique identifier

operatingVoltage

Voltage

Operating voltage

voltageClass

Int32

Primary, Secondary, Unknown

distributionSystemType

Int32

Overhead, Underground, Submersible

geometry

IBoundedObject

Geometric representation

terminals

IEnumerable

List of terminals

specId

Guid

Specification identifier

esriId

Int64

Esri identifier

energizedPhases

Int32

None, C, B, BC, A, AC, AB, ABC, Unknown

phases

Int32

None, C, B, BC, A, AC, AB, ABC, Unknown

facilityId

String

Facility identifier

assemblyId

Guid

Assembly identifier

subnetworkName

String

Subnetwork name

lifecycleStatusType

LifecycleStatusType

Lifecycle status

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?