Geodatabase Region Resource

A Geodatabase Region Resource (GRR) is a JSON file that represents a converted Esri UN model.

Name 

Type 

Description 

id 

Guid 

Unique identifier

feederId 

String 

Feeder ID or Subnetwork Name 

regionName 

String 

Strictly for Geodatabase Region Resources generated via polygon export

patchedDesignId 

String 

Strictly for Geodatabase Region Resources generated during finalizing of the Patch Packet metadata (i.e., used only in case of ADMS Patch Integration for Final GRR data) 

affectedPatchIds 

ISet 

Only for confirmation type of GRRs. This represents the unique set of all design IDs that are going to be confirmed by a specific instance of GRR.

version 

String 

Version number

lastRequestedDate 

DateTime 

Date of last request

lastUpdatedDate 

DateTimeOffset 

Date of last update

components 

Array of IComponent 

Refer to Electric Components for further information.

network 

Dictionary

Represents connectivity of elements, showing everything that is connected to everything else

networkWithTerminalConnections 

Dictionary 

Represents connectivity of elements that have terminals defined, showing everything that is connected to everything else

networkAssociationConnections 

Dictionary

Represents connectivity for nonspatial objects and noncoincident network features

structureRelationships 

Array of StructureRelationship 

Shows structure type (e.g., Container) and topology (parent or child relationship)

tieDeviceInfo

Array of TieDeviceInfo 

Information for tieDevice types of equipment

spatialReference 

SpatialReference 

Defines the coordinate system used to locate the geometry for a feature

referencedSpecs 

IEnumerable 

Strictly for SE ADMS integrations

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.