Additional Configuration Tab in Solution Center

The primary purpose of the Additional Configuration tab is to receive the Storage Service URL. There is one more option, but it differs whether your company also has Designer XI or not.

  • If your company also has Designer XI, there is a toggle to use your existing Designer XI schema for Feeder Services.


  • If your company does not have Designer XI, there is a check box to Use Equipment Specifications. This is an optional configuration, but it allows Feeder Services to integrate with external applications such as Advanced Distribution Management Systems (ADMS) or Outage Management Systems (OMS). See Configure Dynamic Spec Assignment and Feature to Spec Mapping for more information.

    Additional configuration window with the storage service URL text field and Use equipment specifications box.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.