Utility Network with Non-Spatial Units

Non-spatial units in your UN model help manage detailed, heirarchical assets that share a single geographic location.

When units in the UN are not drawn in the map, they are contained by Banks, and the Components used are:

  1. ElectricNetworkComponentBankWithTerminalsResource – this is the bank.

  2. ElectricNetworkComponentUnitResource – this is the unit.

IMPORTANT: One exception is Conductors, for which the modeling didn’t change between the UN and GN. ConductorBank and Conductor should be used in both because they don’t have terminals in the UN.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.