SurfaceStructureResource

Component type used to represent surface structures (pads, pedestals, etc.).

Name

Type

Description

componentType

String

"SurfaceStructure"

id

Guid

Unique identifier

esriId

Int64

Esri identifier

specId

Guid

Specification identifier

facilityId

String

Facility identifier

geometry

IBoundedObject

Geometric representation

workflowState

Int32

[Existing, AsBuilt, Proposed, Undefined, Modified]

properties

IDictionary

Additional properties

lifecycleStatusType

LifecycleStatusType

Lifecycle status

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.