Update Existing Operational Map for Feeder Services

If you already have an existing operational map (for example, one you already use for Editor XI), you can update it to also work with Feeder Services. Follow these steps:

  1. In Solution Center > Mapping > Operational Maps, click the existing Operational Map once to highlight it.

  2. Toggle on GDBM / Feeder Services.

  3. Click Save.

  4. In Solution Center > Feeder Services > Mapping > Map, use the Network Feature Service drop-down to select the operational map. Click Save.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.