FaultIndicatorAssemblyResource

Assembly containing FaultIndicatorWithTerminalsResource devices.

Name

Type

Description

deviceIds

IEnumerable

List of device identifiers

facilityId

String

Facility identifier

componentType

String

"FaultIndicatorAssembly"

id

Guid

Unique identifier

workflowState

Int32

[Existing, AsBuilt, Proposed, Undefined, Modified]

properties

IDictionary

Additional properties

geometry

IBoundedObject

Geometric representation

distributionSystemType

Int32

[Overhead, Underground, Submersible]

esriId

Int64

Esri identifier

subnetworkName

String

Subnetwork name

lifecycleStatusType

LifecycleStatusType

Lifecycle status

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.