ElectricNetworkComponentBankWithTerminalsResource

Generic component class that represents a variety of non-switchable phased electric components that are either uncommon enough that detailed specification data is not available, or simple enough that detailed specification data is not needed.

Name

Type

Description

componentType

String

"ElectricNetworkComponentBankWithTerminals"

workflowState

Int32

[Existing, AsBuilt, Proposed, Undefined, Modified]

properties

IDictionary

Additional properties

id

Guid

Unique identifier

deviceIds

IEnumerable

List of device identifiers

operatingVoltage

Voltage

Operating voltage

voltageClass

Int32

[Primary, Secondary, Unknown]

distributionSystemType

Int32

[Overhead, Underground, Submersible]

geometry

IBoundedObject

Geometric representation

terminals

IEnumerable

List of terminals

esriId

Int64

Esri identifier

energizedPhases

Int32

[None, C, B, BC, A, AC, AB, ABC, Unknown]

phases

Int32

[None, C, B, BC, A, AC, AB, ABC, Unknown]

facilityId

String

Facility identifier

assemblyId

Guid

Assembly identifier

subnetworkName

String

Subnetwork name

lifecycleStatusType

LifecycleStatusType

Lifecycle status

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.