Storage Service Options

The Storage Service is a holding tank that stores cached GIS data from different feature services.

Example: After the Edge Service pulls the feeder and its features, it packages the information into a Geodatabase Region Resource (GRR) file and uploads it to the Storage Service host. When an implementation, such as Outage Management Systems (OMS), wants to consume the GRR file, it can contact the Storage Service and request a download.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.