Geodatabase Regions Error Remediation

If an error occurs during the create or update process, the Availability Status of the subnetwork is set to “Error” and the subnetwork is not available for users. The error is displayed at the bottom of the subnetwork.

The error provides details that led to the process failure. The most common issues include:

  • Temporary Service Outage: This is typically a 500 error produced while the application was trying to reach the feature service. Check to see if services are running, then try again.

  • Environment Issues: These typically involve missing configuration data (for example, a feature service URI) or missing catalog data (components missing equipment specifications). Use the error message to track down the missing configuration data, then try again.

  • Data Issues: These could include unexpected data formats or missing data in the GIS feature class or object table. Use the error message to track down the missing data, then try again.


Hosted Edge Logs

Click the View Logs button. This brings you to the Logs tab pre-filtered to the selected subnetwork. There, you can read more about the error to diagnose the issue. Refer to the Logs topic for more information.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.