TrenchResource

Component used to represent Trench-type GIS features that do not have a geometry.

Name

Type

Description

componentType

String

"Trench"

id

Guid

Unique identifier

esriId

Int64

Esri identifier

workflowState

Int32

[Existing, AsBuilt, Proposed, Undefined, Modified]

specId

Guid

Specification identifier

properties

IDictionary

Additional properties

facilityId

String

Facility identifier

lifecycleStatusType

LifecycleStatusType

Lifecycle status

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.