View the Original Export Subnetwork JSON Data

There are times in which downstream systems from the GIS have existing integrations against Esri’s JSON. Feeder Services provides the identical benefits for GRR maintenance and integration with a new data format. Feeder Services also stores the original Export Subnetwork JSON data alongside the GRR data in the Storage Service.

To view the original Export Subnetwork JSON, perform the following steps:

  1. In Solution Center, click Feeder Services > Mapping > Geodatabase Regions.
  2. On the left side, click the desired GRR once to highlight it in green.

    NOTE: You can use the Search field at the top of Solution Center to search for a GRR by its subnetwork name.

  3. At the end of the Esri Export JSON Storage ID field, click Download file to start a download of the underlying JSON file.

    The file downloads automatically into the Downloads folder of the Windows machine that is running Solution Center. The filename defaults to the name of the subnetwork, and any illegal filename characters are replaced with underscores.

  4. Once the download is complete, click Show in folder to open File Explorer for the newly downloaded file.
  5. Open the file in a text editor, such as Notepad ++.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.