7EN02-0495-01

Command interface overview

The command interface allows you to configure the meter by sending specific command requests using Modbus function 16.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?