Configuration menu for EM3212 / EM3412
|
Section |
Parameter |
Options |
Description |
|---|---|---|---|
|
Wiring |
Type |
|
Select the power system type the meter is wired to. |
|
Frequency |
Frequency |
|
Select the frequency of the electrical power system, in Hz. |
|
Date |
Date |
DD-MMM-YYYY |
Set the current date using the specified format. |
|
Time |
Time |
hh:mm |
Use the 24-hour format to set the time. |
|
Pulse Output |
Pulse Constant |
|
Set the pulses per kWh for the pulse output. |
|
Pulse Width |
|
Set the pulse width (ON time). |
|
|
Contrast |
Contrast |
1 – 9 |
Increase or decrease the value to increase or decrease the display contrast. |
|
Password |
Password |
0 – 9999 |
Sets the password for accessing the meter configuration screens and resets. |
|
Reset Config |
Reset Config |
— |
Settings are reset to their defaults, except for Password. Meter restarts. |