7EN02-0495-01

Power system wiring: EM3700 series

1PH

1PH2W L-N≤ 240 V L-N

1PH2W L-L≤ 415 V L-L

1PH3W L-L-N≤ 240 V L-N
≤ 480 V L-L

1PH4W multi L-N 2CT≤ 240 V L-N

1PH4W multi L-N 3CT≤ 240 V L-N

3PH3W

≤ 480 V L-L

≤ 480 V L-L

≤ 480 V L-L

3PH4W

≤ 277 V L-N
≤ 480 V L-L

≤ 277 V L-N
≤ 480 V L-L

≤ 277 V L-N
≤ 480 V L-L

3PH3W

3PH4W

250 mA fuses and disconnect switch

Shorting block

VT primary fuses and disconnect switch

  • indicates wiring for a balanced system

Clearly label the device’s disconnect circuit mechanism and install it within easy reach of the operator.

Fuses / circuit breakers must be:

  • Installed in accordance with all local and national electrical codes and standards.

  • Rated for the installation voltage, available fault current, and sized for connected loads.

Fuse for neutral is required if the source neutral is not grounded.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?