About this manual
Document scope
Throughout the manual, the term “meter / device” refers to all models of the EM3100 / EM3200 / EM3300 / EM3400 / EM3700 series. All differences between the models, such as a feature specific to one model, are indicated with the appropriate model number or description.
This manual does not provide configuration information for advanced features where an expert user would perform advanced configuration. It also does not include instructions on how to incorporate meter data or perform meter configuration using energy management systems or software, other than ION Setup. ION Setup is a free configuration tool available for download from www.se.com.
Related documents
|
Instruction Sheet |
Number |
|---|---|
| EM3122 instruction sheet |
BRU19330 / BRU19371 |
| EM3212 / EM3224 instruction sheets |
BRU19337 / BRU19377 |
| EM3322 instruction sheet |
BRU19338 / BRU19379 |
| EM3412 / EM3424 instruction sheet |
BRU19339 / BRU19380 |
| EM3712 / EM3724 instruction sheet |
BRU19342 / BRU19381 |
You can download these technical publications and other technical information from www.se.com.