Mechanical characteristics
|
Characteristic |
Value |
Meters |
||
|---|---|---|---|---|
|
IP degree of protection |
Front panel |
IP40 |
EM3100 / EM3200 / EM3300 /EM3400 /EM3700 series |
|
|
Meter body |
IP20 |
EM3100 / EM3200 / EM3700 series |
||
|
Meter body except bottom wiring surface |
IP20 |
EM3300 / EM3400 series |
||
|
Impact rating |
IK08 |
EM3100 / EM3200 / EM3300 /EM3400 /EM3700 series |
||
|
Active energy display range |
In kWh or MWh up to 99999999 MWh |
EM3700 series |
||
|
In kWh: 8 + 1 digits up to 99999999.9 |
EM3100 / EM3200 / EM3300 /EM3400 series |
|||
|
Energy pulsing LED (yellow *) |
500 imp/kWh |
EM3100 / EM3200 series |
||
|
5000 imp/kWh without consideration of transformer ratios |
EM3700 series |
|||
|
200 imp/kWh |
EM3300 /EM3400 series |
|||