7EN02-0495-01

EM3100 / EM3200 / EM3300 and EM3400 series

Functions

Advantages

Can directly measure feeders up to:

  • EM3100 series: 45 A
  • EM3200 series: 63 A
  • EM3300 series: 100 A
  • EM3400 series: 125 A

Embedded current transformers (CTs)

Saves installation time and space in the cabinet

Clear distribution network

Adapted to be installed with Acti9 iC60 (EM3100 / EM3200 series) or Acti9 C120, NG125 (EM3300 / EM3400 series) circuit breakers

Can be used in 3-phase systems with or without neutral

Can be used for single-phase multi-circuit monitoring

3 single feeders can be monitored with a single meter

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?