7EN02-0495-01

RS-485 Base Comm

Configure the Modbus RS-485 communication port settings for the EM3000 series devices. The RS-485 Base Comm port allows Modbus communications with a monitoring and control system, and you can link multiple devices in sequence in a system.
NOTE: We recommend that you do not change the communications settings of the device. If necessary, use the device display to change the device communications settings.
  1. Double-click on RS-485 Base Comm to open the dialog box.
  2. Select a parameter and click Edit to open its specific setup dialog.

    Parameter

    Options

    Description

    Address

    1 to 247

    Enter a value for the address (unit ID) of the device. The address must be unique for each device in a communications loop.

    Baud Rate

    9600

    19200

    38400

    Select a value from the drop down list for the meter's baud rate (speed for data transmission).

    NOTE: The baud rate must be set to the same value for all devices in a communications loop.

    Parity

    Even

    Odd

    None

    Select a value from the drop down list for the communications port parity setting.

    NOTE: That parity must be set to None for all devices to communicate with the ION Setup.
  3. Click OK, and then click Send to save your changes to the meter.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?