7EN02-0495-01

Configuring the meter resets

When you initialize a meter, it will reset or disable certain parameters. Make sure to read the warning message that appears, showing the parameters that are about to be reset.

  1. Double-click on Meter Resets to open the dialog box.
  2. Select Reset All Energies and click Reset.
  3. Click Proceed to reset all Phase energy and Partial energy.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?