Configuring the clock parameters (Date/Time)
- Double-click on Clock to open the dialog showing the list of parameters.
- Select a parameter and click Edit to open its specific setup dialog.
Parameters
Options
Description
Device
Meter Date
Meter Time
Select the meter date and time.
NOTE: The Device changes to Update to and shows the date and time that will be sent to the meter.Sync to
UTC (Universal Coordinated Time)
-
Device time zone
: Not applicable
UTC is the same as Greenwich Mean Time (GMT). Daylight Saving Time and time zones do not apply to UTC.
PC Standard Time (No DST)
-
Device time zone
-
Same as this PC
-
Behind this PC
-
Time Offset
-
-
Ahead of this PC
-
Time Offset
-
-
PC Standard Time is the time on your computer without Daylight Saving Time applied. If the meter you are programming is in a different time zone from your computer, select the appropriate time zone correction.
Select the offset time in hours (0 to 23) and minutes (0, 15, 30, 45). For time zone ahead of this PC, the time is displayed with + sign (example: +6h45min) and time zone behind this PC, the time is displayed with - sign (example: -6h45min).
PC Local Time (DST if applicable)
-
Device time zone
-
Same as this PC
-
Behind this PC
-
Time Offset
-
-
Ahead of this PC
-
Time Offset
-
-
PC Local Time is the time on your computer with Daylight Saving Time applied. If the meter you are programming is in a different time zone from your computer, select the appropriate time zone correction.
Select the offset time in hours (0 to 23) and minutes (0, 15, 30, 45). For time zone ahead of this PC, the time is displayed with + sign (example: +6h45min) and time zone behind this PC, the time is displayed with - sign (example: -6h45min).
Synchronization Time The synchronization time and date of the meter.
-
- Click OK, and then click Send to save your changes to the meter.NOTE: When changes are not saved to the meter, the status bar on the bottom left screen shows Download Incomplete.