7EN02-0495-01

MID/MIR

Characteristic

Value

Meters

Electromagnetic environmental class

E2

EM3224 / EM3424 / EM3724

Mechanical environmental class

M1

For MID/MIR compliance, the Wiring > Type setting must be set to 3PH4W or 1PH4W (Total energy).

The meter complies with the MID 2014/32/EU or MIR SI 2016 No 1153 when installed in cabinets rated for IP51 or better in accordance with the instructions in DOCA0038EN, available on our website. The CE and UKCA declaration documents are available from the website. Search ECDEM3000 for CE declaration document and UKMIREM3000 for UKCA declaration document.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?