7EN02-0495-01

Resets

The following resets are available:

Reset

Description

Partial energy

Clears all active energy accumulated since the last reset.

This does not reset the total active energy accumulation.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?