7EN02-0495-01

Considerations for EM3100 / EM3200 / EM3300 and EM3400 series devices associated with a contactor

Connection requirements for EM3122 / EM3212 / EM3224 / EM3322 / EM3424 / EM3424
  • When the meter is associated with a contactor, connect the meter upstream of the contactor.

  • The meter must be protected by a circuit breaker.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?