Communication
|
Address |
Register |
Action |
Size |
Type |
Units |
Description |
|---|---|---|---|---|---|---|
|
0x1963 |
6500 |
R |
1 |
UInt16 |
— |
Protocol
|
|
0x1964 |
6501 |
R/WC |
1 |
UInt16 |
— |
Address |
|
0x1965 |
6502 |
R/WC |
1 |
UInt16 |
— |
Baud Rate:
|
|
0x1966 |
6503 |
R/WC |
1 |
UInt16 |
— |
Parity:
NOTE: Number of stop bits = 1 and 2
|