7EN02-0495-01

Configuring the alarm parameters for EM3724 series meter

Configure the alarm parameters using the Alarming screen.
NOTE: By default, the alarm is disabled.
  1. Double-click Alarming to open the dialog setup.
  2. Select Standard alarm and click Edit to open Standard Alarm Setup dialog.
  3. Select Over Active Power in the left column to Edit its values.

    Parameters

    Options

    Description

    Over Active Power

    Enable

    Enable or disable the over active power alarm.

    Setpoint Pickup (kW)

    1 to 9999999

  4. Click OK, and then click Send to save your changes to the meter.
    NOTE: When changes are not saved to the meter, the status bar on the bottom left screen shows Download Incomplete.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?