7EN02-0495-01

Modifying a numerical value

When you modify a numerical value, the digit on the far right side is selected by default (except for Date/Time).

The parameters listed below are the only ones for which you set a numerical value (if the parameter is available on your device):

  • Date

  • Time

  • Pick Up Value for an overload alarm

  • Voltage Transformer (VT) Primary

  • Current Transformer (CT) Primary

  • Password

  • Address of the meter

To modify a numerical value:

  1. Use the button to modify the selected digit.
  2. Press to shift to next digit. Modify the next digit, if needed, or press okay to move to the next digit. Continue to move through the digits until you reach the last digit then press again to confirm the new parameter value.
    If you enter an invalid setting for the parameter, when you press after setting the left-most number, the cursor shifts back to the right-most number so you can enter a valid value.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?