7EN02-0495-01

Example: navigating the display screens

  1. Press to scroll through the main display screens; then press to move from Wiring to Frequency.
  2. Press to access additional screens related to main screen (if available); then press to access screens for each of the available wiring.
  3. Press to scroll through these additional screens.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?