7EN02-0495-01

Overview of meter functions

The meters provide the essential measurement capabilities (for example, Active Total Energy and Active Per phase Energy) required to monitor a 1-phase or 3-phase electrical installation.

The key features of the meters are:

  • Measurement of active energy

  • MID/MIR compliance for many of the meters

  • Pulse outputs

  • Display (Energy measurements)

  • Communications using Modbus

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?