7EN02-0495-01

Safety, EMI/EMC and product standards

Safety

BS/ EN/ IEC/ UL 61010-1: 2010 + A1: 2019

BS/ EN/ IEC/ UL 61010-2-030: 2017

Protective class

II

Double insulated for user accessible parts

Standard compliance

IEC 62052-31: 2015

IEC 62052-11: 2020

IEC 62053-21: 2020

IEC 61557-12: 2021

BS/ EN 62052-31

BS/ EN 62052-11

BS/ EN 62053-21

BS/ EN 61557-12

BS/ EN 50470-1

BS/ EN 50470-3

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?