7EN02-0495-01

EM3100 series: 45 A meters

Function

EM3122

Direct measurement (up to 45 A)

Active Energy measurement accuracy class (total and partial kWh)

Class 1

Measurement display (number of lines)

3 Lines

Communications

Modbus

Width (18 mm module in DIN rail mounting)

5

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?