Communications Setup
| Command Number | Action | Size | Type | Unit | Range | Description | 
|---|---|---|---|---|---|---|
| 5000 | W | 1 | UInt16 | — | — | (Reserved) | 
| W | 1 | UInt16 | — | — | (Reserved) | |
| W | 1 | UInt16 | — | — | (Reserved) | |
| W | 1 | UInt16 | — | 1 – 247 | Address | |
| W | 1 | UInt16 | — | 0, 1, 2 | Baud Rate: 
 | |
| W | 1 | UInt16 | — | 0, 1, 2 | Parity: 
 | |
| W | 1 | UInt16 | — | — | (Reserved) |