7EN02-0495-01

The device clock

Only applicable for EM3224 / EM3424 / EM3724 meter models.

You must reset the time to account for any time change (for example, to switch the time from standard time to daylight savings time).

Clock behavior: EM3224 / EM3424 / EM3724

You are prompted to set the date and time when the meter is powered up. Press to skip this step if you do not want to set the clock (you can enter configuration mode and set the date and time later, if required).

When the power is interrupted, the device retains its date and time information for 3 days. If power is interrupted for longer than 3 days, the device automatically displays the screen to set Date & Time when power is restored.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?