7EN02-0495-01

Dimensions

EM3100 / EM3200 series

NOTE: Dimensions are in mm/in.

 

A

Without communications

 

B

With communications

     

EM3300 / EM3400 series

NOTE: Dimensions are in mm/in.
 

A

Without communications

 

B

With communications

     

EM3700 series

NOTE: Dimensions are in mm/in.
 

A

Without communications

 

B

With communications

     

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?