System
|
Address |
Register |
Action |
Size |
Type |
Units |
Description |
|---|---|---|---|---|---|---|
|
0x001D |
30 |
R |
20 |
UTF8 |
— |
Meter Name |
|
0x0031 |
50 |
R |
20 |
UTF8 |
— |
Meter Model |
|
0x0045 |
70 |
R |
20 |
UTF8 |
— |
Manufacturer |
|
0X0059 |
90 |
R |
1 |
Uint16 |
— |
Product ID Number |
|
0x0081 |
130 |
R |
2 |
UInt32 |
— |
Serial Number |
|
0x0083 |
132 |
R |
4 |
DATETIME |
— |
Date of Manufacture |
|
0x0087 |
136 |
R |
5 |
UTF8 |
— |
Hardware Revision |
|
0x0664 |
1637 |
R |
1 |
UInt16 |
— |
Present Firmware Version (DLF format): X.Y.ZTT |
|
0x0723 |
1829 |
R/WC |
1 X 4 |
UInt16 |
— |
Power failure Count |
|
0x0724 - 0x727 |
1830 - 1832 |
R/WC |
1 X 4 |
UInt16 |
— |
Power failure Date/Time:
|
|
0x0734 - 0x0737 |
1845 - 1848 |
R/WC |
1 X 4 |
UInt16 |
— |
Date/Time:
|
|
0xAFC7 |
45000 |
R |
1 |
Bitmap |
— |
Diagnostics error status
|